10/13/2021 9:06 AM | |
Joined: 10/7/2005 Last visit: 10/15/2024 Posts: 3024 Rating: (1054) |
I wouldn't if I were you and here's why and how it can get you into trouble: Assumption 1: The logic inside the higher priority 4ms interrupt OB takes more than 1ms but less than 2ms to execute. Result 1: Execution of the 1ms lower priority interrupt OB gets delayed Assumption 2: The logic inside the higher priority 4ms interrupt OB takes more than 2ms to execute. Result 2: The 1ms lower priority interrupt OB fails twice to be executed, OB80 gets called and your CPU goes to stop |
Cheers |
|
Follow us on