11/3/2016 9:33 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Kicken, no, the default-settings are not depending on the Step7 versions and should be always the same. The most of the modules have a default time of 150ms. I had a look on the default parameters of the FAI6x15bit HART in the manual. It has a default time of 2500ms. so everything is ok. Have a try and set it to the maximum of 10000ms. If the error still occurs, you have to search for other reasons. hope this helps, regards, |
FCK WAR! |
|
Follow us on