8/30/2016 4:45 AM | |
Posts: 1529 Rating: (202) |
Use TIA Portal Network View. All of these components are in my version. |
8/30/2016 5:30 AM | |
Posts: 1529 Rating: (202) |
You need Scout TIA. I think I use HF8, which was a complete installation. I have not done HF11 yet. I would re-install Scout. |
8/30/2016 5:36 AM | |
Posts: 305 Rating: (1) |
this is my TIA vesion . do you use it ? in my system ,use scout tia 、PORTAL to do ,do you can give me some suggest |
8/30/2016 5:59 AM | |
Posts: 1529 Rating: (202) |
I have Scout 4.4.0.8, but it should make no difference. Are you opening your Hardware Catalog in TIA Portal? |
8/30/2016 8:11 AM | |
Posts: 305 Rating: (1) |
this my system . |
8/30/2016 8:58 AM | |
Posts: 1529 Rating: (202) |
With TIA Portal, you need to use Scout TIA. |
8/30/2016 9:24 AM | |
Posts: 1529 Rating: (202) |
I still don't understand the question. You open SCOUT TIA from within TIA Portal. |
8/30/2016 10:27 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
1.) yes with the GSDML you can configure the i-Device Communication 2.) this is not possible 3.) read , read, read ! ther is no GSDML exists for CPU315 DP/PN you must create the GSDML depends on the configuration of the PLC 315 you use! No Standard GSDML available! |
Last edited by: ChristophD at: 8/30/2016 10:30:22 AM |
|
Follow us on