4/24/2019 9:36 AM | |
Joined: 5/12/2006 Last visit: 10/18/2024 Posts: 22422 Rating: (3023)
|
Hello, in the Hwconfig in the PLC properties the webserver can be activated. Which scada you use? Regards Christoph |
4/24/2019 9:43 AM | |
Joined: 11/24/2010 Last visit: 6/7/2021 Posts: 15 Rating: (0) |
Hi, Do you mean in the HW config of D425 or PLC S7-1500? We use Wonderware InTouch. Regards. |
4/24/2019 9:44 AM | |
Joined: 5/12/2006 Last visit: 10/18/2024 Posts: 22422 Rating: (3023)
|
Hi, if you mean the webserver of d425 then i mean the hwconfig of d425 :) Regards Christoph |
4/24/2019 9:49 AM | |
Joined: 11/24/2010 Last visit: 6/7/2021 Posts: 15 Rating: (0) |
Hi again, Thanks so much for the support, Regards |
Follow us on