9/26/2017 12:14 PM | |
Posts: 80 Rating: (1) |
Hi Christoph, I have open the Diagnostic buffer and it shows error 16#F360:BE60 as below quote: "STOP by execution system, cause: Program missing for the task Cause I am not sure what is the missing program it referred to..now i am doing a test to link D435-2DP with a DCM thru profibus. attached is the project file maybe can help to have a look? I want to Assign the DCM as an Axes so it can be used also in the Address List. Azad AttachmentSample_2.zip (56 Downloads) |
9/29/2017 9:46 AM | |
Joined: 6/19/2017 Last visit: 4/25/2024 Posts: 7959 Rating: (162) |
New question published by azad_dsc is split to a separate thread with the subject DCM cannot selected to be assign like a S120. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on