4/26/2019 3:03 PM | |
Joined: 6/28/2011 Last visit: 8/1/2024 Posts: 6 Rating:
|
1.My hardware configuration informatio D425-2 DP/PN 6AU1 425-2AD00-0AA0 V5.2 IM 155-6 PN HF 6ES7 155-6AU00-0CN0 V3.3 TM Count 1x24V 6ES7 138-6AA00-0BA0 V1.3 SCOUT TIA V5.2 2.Fault description M155 does not enable isochronous mode. The hardware connection is normal. There is no abnormality in ONLINE monitoring, but the IM155 enables isochronous mode. The hardware connection is abnormal, and the ET200SP is found. My program is more than 3M, I put it in the DROGBOX, the following connection AttachmentFiles.zip (144 Downloads) |
Last edited by: JHON.H at: 04/26/2019 15:07:07Last edited by: JHON.H at: 04/26/2019 15:30:28Last edited by: JHON.H at: 04/26/2019 16:17:28Last edited by: Jen_Moderator at: 04/30/2019 07:41:24Removed link and added files as an attachment. |
|
4/26/2019 4:27 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
hello, is ok, i will checkthe project on monday. regards christoph |
Last edited by: ChristophD at: 04/26/2019 16:27:51 |
|
4/26/2019 5:04 PM | |
Joined: 6/28/2011 Last visit: 8/1/2024 Posts: 6 Rating:
|
@ChristophD Thank you |
Follow us on