2/29/2024 6:07 PM | |
Joined: 3/14/2008 Last visit: 8/13/2024 Posts: 2084 Rating: (931)
|
Hi, Yes, this is the recommended block. It can create daily, weekly and monthly triggers or single trigger. See attachment for a screenshot. You can set the daily trigger at 12 o'clock as follows:
With the LiOp=0, the operator can set the trigger via SetPerOp/RstPerOp. With LiOp=1, you can set the trigger via CFC by SetPerLi/RstPerLi. You can view the APL help for more info. |
Last edited by: Oreca at: 02/29/2024 18:13:46Last edited by: Oreca at: 02/29/2024 18:54:14If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/6/2024 7:22 PM | |
Joined: 9/9/2015 Last visit: 8/14/2024 Posts: 727 Rating: (277) |
The best way is still NTP time sync. Invest a Cat6 cable, connect to their system and provide the time. Reliable and save commissioning time. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on