11/24/2022 3:15 PM | |
Joined: 7/13/2022 Last visit: 2/28/2023 Posts: 17 Rating: (0) |
Hello everyone, I have a Power Center 3000 which I'm using to collect measurement data from a PAC3220. I'd like to visualize the collected data in SCADA. The POC3000 manual mentions that this is can be done using Modbus TCP (https://support.industry.siemens.com/cs/ww/en/view/109763838 - p126/184 and p142/184). It doesn't give any further instructions though. This left me the following questions: -Which SCADA program should I use? -How can I set up a Modbus TCP connection from SCADA to my device? -Is it possible to not only display values in SCADA, but also collect them and e.g. store them in an excel sheet or other file? I'm looking to make these values (particularly measured current) usable in a C-program. Thank you in advance. Also, I'm not sure if this is the correct place for this question. Could a moderator address this? |
Last edited by: MrPolska at: 11/24/2022 15:15:38Last edited by: Jen_Moderator at: 11/25/2022 07:28:28Link optimized. Last edited by: MrPolska at: 11/25/2022 11:34:59 |
|
Follow us on