Industry Online Support
Technical Forum
8/10/2012 8:53 AM | |
Joined: 2/8/2009 Last visit: 3/5/2023 Posts: 56 Rating:
|
hi friends, I had created programm in S7 400H CPU (414-4HM14-0AB0). I had used STL & FBD language for programming. now we have to use F-IO. We take FDI24XDC24V (326-1BK02-0AB0) IN ET200M (153-2BA02-0XB0). we have CFC optional package and F-package. I make CFC chart and insert F-block (F_:Fail-safe Channel Driver Digital Input) andr connect it with F_DI. but when i try to compile. it gernerate error: FCXX is outside the user range, DBxx is outside the user range. these all FC & DB are my privious programm. if i delete this blocks its compile with no error. my problem is i want my backup as it is (which i had created in STL & FBD language). and want to add CFC with Fail safe chanel driver Block. and want to take Q and QBAD signals of F_DI in my user programm. I am sending my LOG file which gernerate when i compile my CFC. AttachmentLogs.pdf (28 Downloads) |
Follow us on