2/3/2021 3:38 PM | |
Joined: 6/11/2020 Last visit: 9/12/2022 Posts: 2 Rating:
|
Hiya, Is there a way to send data to cloud using WInCC V16 (TIA) Professional? I know WinCC V7.5 had a Data To Cloud Connector but I've not seen anything similar in TIA portal. If there isn't a module, has anyone managed to do it anyway? I've been thinking it might be easier to use a PLC as a MQTT publisher (since I believe there is a library for that) rather than trying to frig it through a SCADA system. I'm not sure how it would work out with the networking but it looks like the easier option atm. |
Last edited by: Jen_Moderator at: 02/04/2021 08:16:08Optimized link. |
|
2/5/2021 8:22 AM | |
Joined: 8/3/2009 Last visit: 8/12/2024 Posts: 13534 Rating:
|
Hello mp-iconsys As I Know the Cloud connector Option is only available for Classic WinCC V7.5. If you have a S71500 then you can use the Library : https://support.industry.siemens.com/cs/de/en/view/109772284 Or you use a Siemens IOT Box. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on