3/12/2012 9:52 AM | |
Joined: 6/28/2007 Last visit: 12/13/2023 Posts: 61 Rating: (4) |
Hi Friends, I am currently using a Data Monitor Server where in i have certain standard WINCC Report which i am printing on timely basis, Also an of this Data Monitor Package is thati can send this report as a mail attachment to recipeints. i have done the required settings as instructed in the Help Manual Provided. But Yet am not able to recieve any email when the report is triggered. I think the forum can be of some help to me here. In th help file there is an comment that we can view if the report email is properly triggered from the PC Can someone help me find out where this is (FROM HELP FILE) "Diagnostics |
Best Regards & Thanks in Advance |
|
Follow us on