3/26/2024 5:42 PM | |
Joined: 3/5/2024 Last visit: 8/15/2024 Posts: 1 Rating: (0) |
Hello Guys, Our company recenty bought a DATALOGIC BC9180-433 base charger (with ethernet connection) device with PM9501 handscanner. It is not supportin Profinet. I wanna connect with my S7-319F CPU I use Simatic Manager with V5.6. The config has no CP just the CPU. I've tried to configure a TCON config, but it is not working. I downloaded an example project from this forum about TCON, TSEND, TRCV. (Entry ID: 29737950 ) I modified the IP adressess and subnets in DB1 the same as datalogic. I tried to start the communication and in the TCON STATUS I did anything and i always get number: 7000. Of course ping is working with the device. The ip adresse ok, In the device's webserver i can see the qr codes. I'dont know what should i config into the PLC's hw configs or other places. Thank you for your help in advance! BR, KHL |
Last edited by: Jen_Moderator at: 03/27/2024 09:52:42Link optimized. |
|
Follow us on