Industry Online Support
Technical Forum
1/20/2010 9:38 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Dear PHILCAT, The OP277 6" has a software clock (not battery backed). So when power is lost, and come back, you will have an old date and time. One possible solution is to synchronize the Date and Time with the CPU. Here is a link which might help: how do you synchronize the date and time between an operator panel and an S7-300/S7-400 controller with WinCC flexible? Best regards, Wizard |
1/20/2010 1:25 PM | |
Joined: 11/25/2005 Last visit: 2/12/2024 Posts: 21 Rating: (0) |
Many thanks for your fast answer |
Follow us on