12/3/2010 3:16 AM | |
Joined: 10/7/2005 Last visit: 5/5/2024 Posts: 3004 Rating: (1046)
|
Hello andrewF your SCL code seems fine, the problem isthe name you used forthe array which you called "id". While this causes no problems for the SCL compiler to create the DB ("id" is a valid element name in a DB), the SCL logic that now tries to access it "complains" because "id" is a reserved keyword for it(ID= English mnemonic for Input Doubleword access). Change the array name from "id" to to something else (e.g. "cant_use_id") and it should all be ok. Below is a "dummy"SCL source (make sure to declare the DB and FB namesin the symbol table before compiling): DATA_BLOCK db_comm_f
|
Cheers |
|
12/3/2010 6:35 AM | |
Posts: 87 Rating: (1) |
big thank you Fritz!!! It help me!!! All works!!! You are best! |
This contribution was helpful to1 thankful Users |
Follow us on