5/18/2012 9:22 AM | |
Posts: 38 Rating:
|
Dear All, I want to know how to export all Content of a DB to Excel and add some data then Import all content from Excel to that Particular DB? Regards Manish |
5/18/2012 9:27 AM | |
Joined: 4/19/2008 Last visit: 10/23/2023 Posts: 1525 Rating:
|
Hello Manish, How do you import an Excel list with STEP 7 variables into a data block? |
Ammy |
|
This contribution was helpful to
1 thankful Users |
5/18/2012 9:30 AM | |
Joined: 9/28/2005 Last visit: 11/6/2023 Posts: 2957 Rating:
|
Hello, You can't do that directly on PLC. You need at least to have HMI capable of logging values. Then you could write them in CSV files and transfer to excel. If we speak about values from excel to DB then you also need a HMI, then write VBS script to read CSV file and update the values in PLC. These links could be of interest: How can you write data to a file or read data from a file by means of a script on a Comfort Panel with SIMATIC WinCC (TIA Portal)? Data transfer via FTP with SIMATIC NET IT-CP |
Best regards, |
|
This contribution was helpful to
2 thankful Users |
5/18/2012 9:31 AM | |
Joined: 9/28/2005 Last visit: 11/6/2023 Posts: 2957 Rating:
|
I suppose question was about runtime values ? Isn't it ? |
Best regards, |
|
5/19/2012 2:14 PM | |
Posts: 38 Rating:
|
Hello Darious Actually I have already prepared the Symbole list of Digital Input & Output in Symbol table and I want to Create Input DB (DB50) for DI & Output DB (DB51) for DO by using the same name used in symbole table. So i Just want to know is there anyway to use the Symbol name of DI directly to that particular DB. |
Follow us on