5/27/2016 1:24 PM | |
Joined: 10/11/2006 Last visit: 5/30/2024 Posts: 5854 Rating: (793)
|
All block connections of data type REAL that are published as BICO parameters are per-unit variables. This means that calculations are performed with per-unit signal values within DCC. (1.0 corresponds to 100%). The conversion to the connector units of the drive is performed automatically. With all other data types, no conversion to a per-unit variable takes place. We would recommend to read the data via a direct connection between HMI and drive. For the HMI-S120 direct connection see following FAQs: https://support.industry.siemens.com/cs/ww/en/view/109481157 |
With best regards, |
|
Follow us on