3/10/2018 5:28 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Hello, If you are able to communicate with S7 PLC then try below point. On PC, in Starter set PG/PC interface as Ethernet, select device unit DCM, set / click on PG/PC as only master on bus, & check. OR If your PC has serial port you can establish communication via serial port. But it won't work with USB to serial converters & AOP30 must not be connected to drive. Please refer attached sheet for serial interface. HTH. Attachment6RA80 STARTER serial communication.pdf (377 Downloads) |
Last edited by: PISCEAN 2010 at: 3/10/2018 5:36:19 AM |
|
3/14/2018 7:22 AM | |
Posts: 69 Rating: (4) |
How to communicate PLC and DCM for encoder feedback? |
3/15/2018 5:57 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Could you please explain your requirement in details? e.g. what you want to achieve? |
3/15/2018 11:52 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Please refer SINAMICS DCC: Positioning and synchronism with SINAMICS DCM and CU320-2 example. |
Last edited by: Jen_Moderator at: 3/15/2018 1:33:54 PMOptimized link. |
|
3/15/2018 1:14 PM | |
Posts: 69 Rating: (4) |
CU320-2 is an additional module to be added ? |
3/16/2018 6:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
In this application, CU320 acts as technology CU & controls the application. Please refer Motion Control Applications with SINAMICS DCM 05/2017 (1,7 MB) document. |
Last edited by: Jen_Moderator at: 3/16/2018 10:15:25 AMOptimized link. |
|
3/16/2018 6:03 PM | |
Posts: 69 Rating: (4) |
Yea I have referred the pdf. So can't I control the drive with position feedback without this CU320 board? |
3/19/2018 12:51 PM | |
Posts: 69 Rating: (4) |
How to do that without CU320? |
Follow us on