11/21/2010 6:10 PM | |
Posts: 18 Rating: (0) |
Hi I want to debounce digital input to stop my plant from faulty random short loose connection.I want to dot it in haedware. |
11/22/2010 6:38 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello hextalker you can only do it in HWconfig if the DI card supports it (e.g. interrupt capable ET200M DI, High feature ET200S DI etc.), so the question is: What type of DI card (part number) do you have? |
Cheers |
|
11/23/2010 10:51 AM | |
Posts: 18 Rating: (0) |
Hi I am using 6ES7 321-7BH00-0AB0 .It is also configureable online, is it CIR compatible/ thank you |
11/23/2010 12:04 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305)
|
Hello hextalker, Yes, it is. You can read the following in the CIR manual*,
A 20msec delay may and may not solve your problem. If it's still not sufficient then you will have to go with ON delay timers as suggested by hdhosseini. * if you have STEP7 V5.5 then thiswill be your CIR manual. Best regards, H-H |
Follow us on