8/17/2023 2:31 PM | |
Joined: 7/7/2023 Last visit: 9/26/2023 Posts: 5 Rating: (0) |
Hello, We have to migrate a S5 PLC and integrate the software into an existing S7 PLC To do this I want to make sure the IO area as well as the Memory are doesn't overlap between the two PLCs and correct the ones that do. However the assignment list in simatic manager does not display the declared but unused tags (see attachment) only the ones that are used. Is there anything I can do show them in the S7 assignment list or if not, is there another way to check the IO & memory areas overlap. Thank you. AttachmentUnused tags ticket.zip (273 Downloads) |
Follow us on