11/1/2018 4:54 PM | |
Joined: 6/4/2010 Last visit: 8/5/2024 Posts: 386 Rating:
|
Dear Vasia, A firmware update for the Control Point PXM50-E is in development. Various performance improvements are planned. Please note that there is one known issue with a workaround. You can find detailed information in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/109757089 Symptoms Delayed reaction of the user interface during navigation or operation in DCP: Navigation from page to page through customer projects takes several seconds. It takes several seconds until the values will be updated in the list view. Slow reaction during command an object. Update of a graphic page takes more than 20 seconds or leads to a crash. Slow reaction during engineering of graphic pages.
During engineering of graphic pages programs will be duplicated during some special manipulation ( e.g. copy of an object). This programs runs during operation of the customer and leads to performance problems.
Until a solution will be released and the duplication of the programs will be denied, the programs needs to be removed manually.
Albis AttachmentWorkaround_deleting_Programs.pdf (466 Downloads) |
Follow us on