1/9/2023 5:31 PM | |
Joined: 12/20/2022 Last visit: 1/10/2023 Posts: 4 Rating:
|
Here attached goes a screenshot of the print preview. |
1/10/2023 10:00 AM | |
Joined: 4/28/2015 Last visit: 4/9/2024 Posts: 94 Rating:
|
Hi, did you check if a Quality update is available for your Desigo CC version? Best Regards, |
3/20/2023 4:46 PM | |
Joined: 6/4/2010 Last visit: 7/16/2024 Posts: 383 Rating:
|
Dear forum member, This issue was related to a specific Microsoft update. Please read the Microsoft kb5022083 for detailed information. See: Imporant part is: “Resolution This issue was addressed in out-of-band updates released January 31, 2023, for Windows 10, version 1607 and Windows Server 2016 versions and newer operating systems and out-of-band updates released February 17, 2023 for earlier Windows and Windows Server versions. To get the standalone package for these out-of-band updates, search for the KB number in the Microsoft Update Catalog. You can manually import these updates into Windows Server Update Services (WSUS) and Microsoft Endpoint Configuration Manager. For WSUS instructions, see WSUS and the Catalog Site. For Configuration Manger instructions, see Import updates from the Microsoft Update Catalog. If you used any workaround or mitigations for this issue, they are no longer needed, and we recommend you remove them. To remove workaround review the workaround or alternative workaround which was applied for instructions.” Best regards, Albis |
Follow us on