Industry Online Support
Technical Forum
9/23/2024 6:49 AM | |
Joined: 10/12/2023 Last visit: 9/26/2024 Posts: 28 Rating: (1) |
Hello Albis, Is it possible to add several exclusions in one event cause field? Performing various tests, nothing comes out. What I want is not to receive notifications about backups and transaction modes. When I add another backup rule, it overwrites the previous one. It would be great if it could be saved in one field, but my tests show it is probably impossible. The client only wants serious system alerts (which come under the information category). ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/23/2024 08:54:23New subject after splitting |
|
Follow us on