9/15/2024 10:18 AM | |
Joined: 9/15/2024 Last visit: 10/16/2024 Posts: 2 Rating: (0) |
We are experiencing a recurring issue with the DI 16x230VAC 6ES7521-1FH00-0AA0 channels in some of our remote I/Os in the field. These channels are frequently getting damaged. When a channel is damaged, it exhibits flickering behavior, turning on and off at a high frequency. Upon checking the current, I found that the damaged channels are drawing less than 4 mA, while functioning channels should show a current greater than 10 mA. What could be causing this issue, and how can we protect the channels to prevent further damage?
Attachmentdamaged channel.avi (86 Downloads) |
Follow us on