11/18/2006 2:00 PM | |
Posts: 122 Rating:
|
[:(]dear experts: i want to know what is the function of "diagnostic address"of a node in profibus DP MASTER SYSTEM,and i find that if there is a node of ET-200 whose "diagnostic address"is 16376(show in the inside document of 001 in my archived document),then it's "I address"is 16375(document 002). but non-ET200 nodes only got "diagnostic address",so what is the difference of profibus "diagnostic address"between these two nodes? Attachment1.zip (771 Downloads) |
11/23/2006 8:14 AM | |
Posts: 122 Rating:
|
simatic PCS7+SP1 with intergrated STEP 7 V5.2+HF5 |
Follow us on