5/19/2015 10:03 AM | |
Posts: 26 Rating: (0) |
Hello expert, after a conversion of a project Scout 4.4 to TIA i can't find the diagnostic adress of an i-device. I need it because in the my first machine the i-device slave is not used so i need to disable it. Where is it? Or it was lost?
|
Last edited by: Min_Moderator at: 5/19/2015 10:46:37 AMNew subject after splitting |
|
5/19/2015 10:22 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, where is the idevcise GSD?
|
5/19/2015 12:08 PM | |
Posts: 26 Rating: (0) |
Sorry, the i-device is reverse, in the D4x5 project is configured a PLC as slave. The GSD of PLC i-device was imported in the D4x5 Scout project. This was made in Scout version 4.3.1.9 and now in TIA i can't find the diagnostic address of this PN slave AttachmentSlave i-device.zip (129 Downloads) |
1/19/2016 2:47 PM | |
Joined: 9/29/2008 Last visit: 3/1/2024 Posts: 7 Rating: (0) |
Hi ChristophD, yes the deactivate function works in scout 4.4 classic configuration, and not in scout Tia. Our config is a 315-2 PN configured with some I-device data Exchange words, exported GSD and imported in a Tia Portal configuration using a D445-2 with Scout Tia. Bye AttachmentArchive.zip (116 Downloads) |
Follow us on