Industry Online Support
Technical Forum
7/24/2013 10:31 AM | |
Posts: 1547 Rating:
|
Hi, yes it is complete different for S7 300 and CP. I suggest using the internal interface and using the PNIO-Diag Option which will fulfill your entire requirement. There exists already a sample also with winCC or winCC flexible. Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO With CP you must program a complex program by using the PN Functions of SIMATIC NET library and you must test the functions. It is cheaper using existing library and samples. |
Follow us on