6/29/2009 12:35 AM | |
Posts: 2 Rating: (0) |
Can not configure a Profibus Diagnostic Repeater with a S7 315 CPU and ET 200M to read its diagnostics on the S7 program..please need some help |
6/29/2009 6:45 AM | |
Posts: 262 Rating: (45) |
Hi, You have to see if you are using OLM routing. refer the below manual for connecting ET200 station with a Salve CPU via Master CPU. https://support.automation.siemens.com/WW/llisapi.dll?query=6ES73988RA008BA%29&func=cslib.cssearch&content=skm%2Fmain.asp%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8 AttachmentDetails of Manual reference.zip (142 Downloads) |
6/29/2009 7:06 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello, Perhaps this will helps. http://support.automation.siemens.com/WW/view/en/24253536 Regards Hristo Mihalev |
6/29/2009 9:39 AM | |
Posts: 160 Rating: (16) |
Please have a look at the following link on how to read in and display diagnostics. This is what you will need to read the diagnostics in your S7 program. BTW what modules are you using in your ET200M station, do they actually support diagnostics. Can you please provide us your hardware config for review? http://support.automation.siemens.com/WW/view/en/387257 Refer to the following link for a manual on how to use the diagnostic repeater. http://support.automation.siemens.com/WW/view/en/7915183 |
Follow us on