3/31/2017 11:15 AM | |
Posts: 1 Rating: (0) |
Hi all, I am starting programming Siemens drivers and I just learn it. I have problem with diagnostic et200m module with cp341 by profinet. I used SFC51 "RDSSYST" in OB1, but I don't know parameters. I can't use B2 in SZL_ID, because et 200m is on other rack. When I use B3 or B1 or B4 any diagnostic address doesn't work. Always I have error 8083 in RET_VAL parameter. In Index parameter I tried all possibilities I think. I search a lot of answer, maybe I should use another function? But what, from all what I found, SFC51 is the best, I think. Thank you for answers.:) I attached my program. AttachmentDiagnostic.zip (39 Downloads) |
Follow us on