12/26/2016 9:55 AM | |
Joined: 7/20/2011 Last visit: 3/22/2020 Posts: 1 Rating: (0) |
Dear Kriipc, Dear all, I am looking diagram connection between S7-1200 and Mitsubishi servo drive. I have connected as in your diagram but the Servo can not run when having pulse output form S7-1200. I worry if it has any wrong. Because when having direction output, Servo will get this signal direction . But PP pin will have signal also. I think so. Pls help me some ideas Thanks and best regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/27/2016 11:44:35 PMNew subject after splitting |
|
12/27/2016 11:45 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by AutoGen_919322 is split to a separate thread with the subject Servo amplifier mitsubishi mr-e-70a plug on a plc siemens s7-200. Best regards |
Follow us on