5/14/2014 6:54 AM | |
Posts: 81 Rating: (1) |
Any body knows the difference between them |
5/14/2014 6:01 PM | |
Posts: 2661 Rating: (279)
|
Hi umair, Open PCS7 is a PCS7 OPC server product (suite). Similarly WinCC is also an OPC server product. See the following manual for description of Open PCS7: http://support.automation.siemens.com/WW/view/en/36183293 On the other hand SIMATIC OPC Scout is an OPC client to connect to/test various OPC servers like Open PCS7 OPC server, WinCC OPC server or any other third party OPC server (for example Matrikon). Regards |
This contribution was helpful to1 thankful Users |
4/29/2020 1:11 PM | |
Joined: 7/31/2014 Last visit: 6/6/2022 Posts: 10 Rating: (3) |
The link is unfortunately now dead. |
4/30/2020 12:29 PM | |
Joined: 9/9/2015 Last visit: 6/7/2024 Posts: 727 Rating: (270) |
The link is wrong one. I think this link will be the correct link. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on