12/26/2015 2:37 PM | |
Posts: 163 Rating: (2) |
Hello, I need to know the difference between Simatic Thin Client and Simatic Multi Panel? Regards, |
12/26/2015 5:38 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, A multi panel is a HMI device loaded with a HMI project created with WinCC configuration software. The multipanels have successor types being the comfort panels. |
Best regards |
|
12/27/2015 8:02 AM | |
Posts: 163 Rating: (2) |
Thanks for the reply. Which one of them could be used as operator station OS for PCS7? Regards |
12/27/2015 10:06 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, An OS for PCS7 is typically a PC/a server running WinCC software. A thin Client could be a kind of remote screen for a PC/a server running WinCC. Look here A comfort panel cannot run the WinCC software needed for PCS7. But there is an FAQ about: |
Last edited by: jklm at: 12/29/2015 6:21:08 PMFAQ about integration of comfort panels Best regards |
|
This contribution was helpful to1 thankful Users |
1/7/2016 3:07 PM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
A thin client is used in implementing distributed HMI solutions with client-server architecture. The following Application shows very good how to install an SIMATIC Thin Client. Decentralized Operation of SIMATIC WinCC with SIMATIC Thin Clients |
Follow us on