5/25/2016 9:52 AM | |
Joined: 1/14/2016 Last visit: 1/13/2022 Posts: 3 Rating: (0) |
Hi, Can you explain me how different when I make connection with two LOGO in network project and in "tool-->Enthernet Connection". Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/25/2016 11:18:19 AMNew subject after splitting |
|
5/25/2016 10:30 AM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33840 Rating: (4206)
|
In network project, you can not not be used under "Tools> Ethernet Connection" the function of generating a connection, it is grayed out (first example). In network project to create a connection to a partner (HMI, S7, Handy, etc.) (fourth example). Example videos attached. Attachmentscreen_video_examples.zip (563 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on