7/22/2023 10:17 PM | |
Joined: 6/11/2019 Last visit: 8/31/2024 Posts: 2227 Rating: (99) |
hello Auto_Gen ..., In the Logo you have a gifted address range (0-850) where you can write and read via network in and out of the VM memory from the Logo program. In addition, it is possible for external devices to query the status of the inputs and outputs (including the network) directly. You can also control flags and outputs directly (without a logo program) if they are not controlled by a program on the logo. You can find a list of known addresses here. greeting Ella_68 (translated with Google) |
Follow us on