9/14/2008 1:40 PM | |
Joined: 9/27/2006 Last visit: 12/7/2023 Posts: 12188 Rating:
|
hello Ayman; This is simplifying things a little bit. In the Simatic Net Profibus networks manual (profn2_e.pdf), in the Passive Components for RS-485 networks chapter, you will find tables showing the different Profibus cables offered by Siemens and their main differences. I have taken the liberty of reducing the table to the simplest distnctions between cables: · FC Standard Cable · FC FRNC Cable: halogen-free FRNC sheath material · FC Food Cable: Sheath material PE 8.0 +/- 0.4 mm; UV resistance; flammable · FC Robust Cable: flame-retardant according to VDE 0472 T804 test type B; good resistance to mineral oil and greases; UV resistance; UL listed · FC Underground Cable: Sheath material PE/PVC 10.8 +/- 0.5 mm · FC Trailing Cable: Repeated bending radius ≥ 60 mm. Cable suitable for applications involving torsion: min. 5 million torsion movements on 1 m cable length (+/-180o) · Festoon Cable: Unrestricted segment lengths; Cables capable of trailing for the following requirements:- min. 4 million bending cycles at the specified bending radius (≥ 70 mm ) and max. acceleration of 4 m/s2 · Flexible Cable: repeated bending radius ≥ 120 mm. Cable suitable for applications involving torsion: min. 5 million torsion movements on 1 m cable length (+/-180o) · FC Process Cable for IEC 61158-2 (Profibus-PA): d.c. loop resistance ≤ 44 Ω /km; Transmission rate 31.25 Kbps, cable corresponds to FISCO model · SIENOPYR FR Marine Cable: very good resistance to mineral oil and greases; Operating temperature -40°C + 80 °C If you go to Profibus.com and Search the Product section for CABLE, you will return more than 300 hits from different manufactures (Phoenix Contacts, moeller, Profichip, Belden...) that can be used in specific environments. I have had to work in applications that required trailing cable, we needed it on a drum roll that would unwind as the platform it was connected to moved away, and rewound as it came back. Standard Profibus cable would never have survived the repeated twisting and bending on the winder; we found out by experience, the maintenance crew had used some on one of the units during a shutdown test; the cable cores broke after a couple of hours. Replacing the cable with braided, more flexible wires (Trailing cable) fixed the issue and ensured that all other specifications for Profibus cable were maintained. So standard cable will always be the "normal" cable used in Profibus networks and the first choice. But for any specific environmental or process applications, there are always alternatives you can apply. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 9/14/2008 1:41 PM |
|
9/15/2008 10:33 AM | |
Joined: 5/28/2008 Last visit: 12/5/2023 Posts: 4486 Rating:
|
Thanks dchartier. |
Ayman Elotaify |
|
Follow us on