3/27/2020 8:14 AM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Hi, Probably the best manual is "What's new" manual. See Link PS: at this moment the website is in maintenance, so I cannot point you to the manual itself. But in the link under tab: "Introduction" you can find the manual. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
3/28/2020 3:46 AM | |
Joined: 9/9/2015 Last visit: 7/24/2024 Posts: 727 Rating:
|
Let me share 4 points. If ppl asked me this question, comparing >PCS 7 V8.2/9.0 and PCS 7 V<8.1, 7.0, 6.0, To me, I think they are almost similar, but the probability of having bugs getting lesser. 1. WinCC - startup faster, WinCC tag management , taglogging, alarm logging, etc interfaced changed to more user friendly. 2. APL - One of the best features I like the most, Ctrl+left click on the APL Block icon to call up APL trend Page. Eliminate the effort to configure customized trend page one by one. You can compare trends of LIT, PIT, FIT relationship just by Ctrl + Click. 3. CFC chart, come with "Avoid dead time " function. You could enable the function to make your program run sequence arranged automatically when you do programming. 4. Compatible to newer window, probability of crashing lesser. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
2 thankful Users |
Follow us on