9/29/2018 8:04 PM | |
Joined: 10/27/2015 Last visit: 10/22/2020 Posts: 60 Rating: (0) |
Dear Everybody! I recognize a different symptoms on FS4 FW1.81.01. In my case at long term operation PLC handling and front panel are freeze, but the web display always works fine and show the real data of moment of freeze (IO ….). The symptoms are same in case of 24V (ext pws) and 230V LOGO!8. Anybody recognize this problem too? Can fw upgrade solve it? Thanks for any advise.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/1/2018 9:36:09 AMNew subject after splitting |
|
9/29/2018 8:34 PM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32974 Rating: (4076)
|
Everything is written about this theme. Which answer do you expect? |
9/30/2018 8:09 PM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32974 Rating: (4076)
|
Did you make the firmware update? This update also fixes other bugs. And if that does not help, start a Support Request. |
10/2/2018 10:05 AM | |
Joined: 9/19/2018 Last visit: 5/6/2024 Posts: 376 Rating: (46)
|
Yes, you should update the firmware of your LOGO!. See following link: https://support.industry.siemens.com/cs/ww/en/view/109750845 Your LOGO! Support. |
This contribution was helpful to1 thankful Users |
10/2/2018 10:58 AM | |
Joined: 12/18/2014 Last visit: 5/6/2024 Posts: 32974 Rating: (4076)
|
Thank you for confirming my statement. |
Follow us on