2/21/2022 4:05 AM | |
Joined: 12/18/2014 Last visit: 5/26/2024 Posts: 33108 Rating: (4087)
|
The information in the TIA Selection Tool only refers to the inputs and outputs on the base module itself. However, with the appropriate expansion modules, a LOGO! Basic modules but manage the following: - 24 digital inputs If several LOGO!s 0BA8 are networked, even more inputs and outputs can be processed with the appropriate expansion modules. AttachmentLOGO! 8 manual 0BA8 2021_05 xxxx8-0BA1 pages 29-31.pdf (526 Downloads) |
Last edited by: ixo65 at: 02/21/2022 05:07:27Attachment |
|
This contribution was helpful to1 thankful Users |
Follow us on