11/21/2010 6:29 AM | |
Posts: 5 Rating: (0) |
Hi Ayman, Thanks for the mail. The module number is 6ES7 322 1BL00 0AA0. The output LEDs are not lit as mentioned earlier. Best Regards Suresh |
11/21/2010 4:41 PM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (309)
|
Hello SureshNair, Please check your wiring as the gentlemen advised. Check your ground (Zero volt). Measure the volt across the relay coil. Try taking out the coil from the relay base and measure the volt across the terminals of the base (wires) while the digital output is off. - If you are still measuring some volts then you have a wiring problem. - If the reading is gone then it's a problemin your coil that's building some energy that's not quickly dissipated. Try using freewheeling diode and see if it gets better. Best regards, H-H |
Follow us on