12/5/2013 11:28 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello You can consider using SIPLUS_RIC With IEC-103 and use a S7 OPEN MODBUS TCP/IP library running in one S7 CPU ( I feel even IM151-8 might be sufficient for your application. ) Of course you need to be familiar with S7 programming if you wish to use SIPLUS RIC libraries. We have had good experience with SIPLUS RIC Libraries as well as MODBUS TCP/IP Libraries. Though we have never used both together in one CPU. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on