4/11/2016 9:55 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Well, you can customize the icon in the way you want. You can make a copy of the existing VlvMotL icon and rename the icon to for example: "Monitor". Then you can delete several objects from the icon so the icon only shows what you need. You will have to test the icon (apdiag.exe) to check for errors. In the AS block, you refer to "Monitor" block icon and after generating, the icons are created for all your AS blocks which have the "Monitor" icon. Another way is to customize your AS block. You can do a lot by using the "OS_Perm" and "Feature" parameters like disabling operator functionalities. Also, you can disable alarms and such. |
Last edited by: Oreca at: 4/11/2016 9:57:41 AMIf I could help you, you can use the RATE button. Thank you. |
|
4/11/2016 11:51 AM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928) |
Which I mentioned in my post also |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on