5/13/2025 1:40 PM | |
Joined: 6/1/2006 Last visit: 6/12/2025 Posts: 137 Rating:
|
Hello DanielM4dsen, |
5/15/2025 10:11 AM | |
Joined: 5/13/2025 Last visit: 5/15/2025 Posts: 2 Rating:
|
Thank you for your time! Yes, correct, that might be the right question to ask. But we've used that function and then we get a system alarm when it is disabled, that says: "Error: Error on partner - No neighbor could be detected... " And I've been looking into using ReconfigIOSystem, but when I put the connection to "Set Partner by user program" the code cannot be compiled, with the error: "For multiple use IO systems or standard machine projects, all specified partner ports are limited to partner ports of their own IO system. All devices have to support topology" As I understand it, this allows me to configure the partner port, and if I configure it to 0 and the partner is disabled, it should work. But it is not possible to get to testing it. |
Follow us on