11/9/2011 5:01 PM | |
Posts: 18 Rating: (0) |
Thanks Wizard, that works great. |
11/9/2011 11:05 PM | |
Posts: 18 Rating: (0) |
Yes, Wizard helped with ONE problem, but there are many more trust me. I'm not at all happy with the LAD editor, data type checking errors, and data type limitations. And I'm not going to list every problem here. But here's one for you since you seem interested: why can't Ichoose DINT on the input parameter for T_CONV in LAD (see screenshot) in V11? This Siemens support link showsa DINTbeing used in their examplehttp://support.automation.siemens.com/WW/view/en/48711306 It's stuff like this which makes this LAD editorhorrible in my opinion compared to others on the market. In your post, you wondered what the-new-kids-on-the-block will do...I hope they use Controllogix and save themselves some frustration. |
Last edited by: garf123 at: 11/9/2011 11:16 PM |
|
11/10/2011 11:02 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello garf123, Can you explain which version you have exactly. Here you can download Service Pack 1 and latest updates: Service Packs 1 for STEP 7 V11 and: Service Pack 1 for WinCC V11 Updates for STEP 7 V11 SP1 and WinCC V11 SP1 Best regards, Wizard |
11/10/2011 3:50 PM | |
Posts: 18 Rating: (0) |
@Wizard: To answer your question, I believe my software versions are up to date (see attached). Siemens Tech Support had me do a "Repair installation" from the CDROM (TIA V11 + SP1)last week to get rid of some SQL errors I was having on migration of projects from the old software(V5.4 + SP5). Perhaps I need to reinstall Update2 now, although the software still reports that Update2 is installed. I don't know.All I know is thatI think Siemens should rename "Migration" to "Migraine" because of how much of a hassle it is, unlike other PLCs like AB where it is much better (e.g. importing old APS and AI files into RsLx500 by just selecting File\Open\ *.ACH). |
Last edited by: garf123 at: 11/10/2011 11:11 PMLast edited by: garf123 at: 11/10/2011 4:52 PMLast edited by: garf123 at: 11/10/2011 4:11 PMLast edited by: garf123 at: 11/10/2011 4:06 PM |
|
Follow us on