5/17/2013 11:46 AM | |
Posts: 68 Rating: (7)
|
Dear users of the Siemens Industry Online Support, Welcome to the forum thread on the FAQ„How in STEP 7 (TIA Portal) V12 do you migrate the call of the instruction "RDSYSST" (SFC51) from S7-300/400 to S7-1500?“. Here you have the opportunity to scrutinize the solution presented in the FAQ, to amend it and to discuss other solutions. We are looking forward to your feedback and your comments. |
Last edited by: FAQ-Expert at: 5/17/2013 12:29 PMLast edited by: FAQ-Expert at: 5/17/2013 11:53 AM |
|
5/17/2013 12:24 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating: (1438)
|
Hi, who comes to this FAQ could also be interesting in general diagnose features of S7-1500. In this context I suggest take a look also in the tread "TIP: S7-1500 Diagnose" at https://www.automation.siemens.com/BR/tf/WW/en/Posts/89419 |
Denilson Pegaia |
|
5/21/2013 11:09 PM | |
Posts: 74 Rating: (31) |
Hi, As the FAQ doesn't give a direct explanation on how to use RDREC for substituting some of the RDSYSST functions, uou might have a look at this thread: It explains how to read out things like Serial Number, S7 Article Number, MAC Address, Profinet Name, etc. And most important - how to find which hardware ID number to feed the RDREC function with. And a general note about those FAQ discussions: Would it be possible to add or change the subjects of these threads to a more describing name? It is difficult to get an overview with all those FAQ numbers in the forum list. Maybe the FAQ-discussions should be moved to a sub-groub so the product family groups won't be flooded. Discussion on the <-- This part is redundant - everything in this forum is more or less a discussion! FAQ68397488 <-- The number doesn't say me anything... It might work for searches, but that's about it. I understand that the original title of the FAQ might be too long. An optimal subject could be: FAQ: How to migrate theS7-300/400instruction "RDSYSST" (SFC51) to S7-1500 or: FAQ68397488: RDSYSST (SFC51) in S7-1500 using TIA
|
This contribution was helpful to1 thankful Users |
5/22/2013 2:37 PM | |
Posts: 68 Rating: (7)
|
Dear Jorsal thank you very much for your post in general and for the note about our new FAQ discussions in particular. We're right into a public test of those discussions, so we're pleased to get some feedback. Some of the mentioned topics are known issues and are caused by technical limitations, some of them are new to us as well. Be sure: We'll check all of your suggestions in detail. Thank you for helping us to improve our service! |
This contribution was helpful to1 thankful Users |
Follow us on