2/5/2024 8:21 PM | |
Joined: 10/6/2022 Last visit: 5/20/2024 Posts: 12 Rating: (0) |
I am trying to achieve exactly the same outcome. I am also having trouble getting information to display in the diagnostic window on the TP700 HMI. When you talk about integrated connection, is that the HMI connection established in Device view? Is this connection setup correctly (see screenshot)? Once established will i see all hardware connected to the PLC - remote io, VSDs, encoders etc? ------------------------------------------------------------------------------------------ |
Last edited by: ENRM at: 02/05/2024 20:22:28Last edited by: Jen_Moderator at: 02/07/2024 09:13:39New subject after splitting |
|
2/13/2024 12:04 PM | |
Joined: 8/3/2009 Last visit: 6/19/2024 Posts: 13078 Rating: (1660)
|
Hello ENRM check out this FAQ: https://support.industry.siemens.com/cs/de/en/view/89852595 If you are not sure check your HMI connection Editor here you hae to see soemthing like this in front of the connection: Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/13/2024 5:28 PM | |
Joined: 10/6/2022 Last visit: 5/20/2024 Posts: 12 Rating: (0) |
These are the connections i have in the project |
2/13/2024 5:54 PM | |
Joined: 10/6/2022 Last visit: 5/20/2024 Posts: 12 Rating: (0) |
Project login User name: User Password: Sieportal AttachmentSiePortal2.zip (112 Downloads) |
2/14/2024 10:04 AM | |
Joined: 10/6/2022 Last visit: 5/20/2024 Posts: 12 Rating: (0) |
Hi, Thank you for your reply. This is what i have. |
2/14/2024 10:04 AM | |
Joined: 10/6/2022 Last visit: 5/20/2024 Posts: 12 Rating: (0) |
HMI - Connections |
Follow us on