10/30/2006 9:35 PM | |
Posts: 1275 Rating:
|
Not right now.... [:(] anyone? I'm gonna do some research, and I'll post if I come up with something! |
This contribution was helpful to
1 thankful Users |
10/31/2006 9:30 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Firstly have you set the standard server on the client as detailed in this FAQ? I think you need to do this. I don't have time to test but these are my current thoughts :-do remember that if you are displaying a PDL from the server then it will have a server prefix which is applied to all tags. So all tagson the picture arecalled from the server. This is not what you want but it is what is configured. If you want local tags such as @CurrentUser displayed then try using @local::@CurrentUser instead. The @local:: prefix tells WinCC to use the local copy of the tag and not the servers copy. This is more a PCS7 thing so maybe one you PCS7 guys can confirm the exact syntax if I have it wrong. I am tied up most of this week (dared to take a holiday and know dealing with the work backlog [:(] ) but we should be able to get this one bottomed out soon. |
This contribution was helpful to
3 thankful Users |
Follow us on