5/13/2016 2:51 PM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Dear PCS7 Experts, In PCS7 (V8) you can define a text library for use in alarms. In our case we use it for the detailed description of drive alarms. For an alarm we can use this textfrom user text libraryusing the following syntax “@3W%t#TextLibName@”, where 3 is the index within the text library and TextLibName is the name of the text library. Our problem is that we also want to display a text form the user text library on a WinCC page (for example in a multi row text control) by specifying:
It is not available as an internal tag, like a regular enumeration. We also have looked through the available C-script functions and ODK, there seems to be no functions available to access the user text library. Do you know if this is possible? Note that we don’t use the regular enumeration because the texts we have to define are much longer than allowed (>16characters). Hope somebody can Help! Kind regard, Jaap |
5/13/2016 7:46 PM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi Jaapie, I don't know exactly what you mean yet, but I've used the following FAQ once. Maybe it's useful for you!? Regards, Oreca |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/19/2016 11:16 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi Jaapie, Thx for the feedback, even if it was not too helpful. Normally, I'm not fund of sending links to FAQ's and say: "You can find the info here, look into it yourself", but I did some searching and found maybe some interesting stuf. Maybe it's more useful to you...Otherwise, I have to leave this to someone else Fill combobox with text library contents There is a .zip file above figure 4 under the following link, which may be useful. Hope you can solve your issue! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on