Industry Online Support
Technical Forum
8/29/2011 11:28 AM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating:
|
Hi bermuda, I think you need a protocol gateway like this one http://kalkitech.com/offerings/sync-field_protocol_io_gateways/ Hope this can help a bit, BV |
11/28/2013 1:24 PM | |
Posts: 3 Rating:
|
Hello Bermuda, BeVee, Our SYNC 2000 can be used to connect the DLMS meter(where the meter can be connected directly to the RS485 port on our SYNC 2000 protocol converter, or if multiple meters needs to be read, they can be multidropped in daisy chain) to the Modbus master device We have successfully completed numerous projects integrating DLMS Meters to the master devices(which are on Modbus, IEC61850, DNP3, etc) Here is the link of case study of the recent project which we completedhttp://www.kalkitech.com/documents/SYNC%202000%20Protocol%20Gateway%20V2_Case%20Study.pdf, where we integrated DLMS meters to IEC61850 SICAMPAS system Best Regards, Gautam Bhat |
Last edited by: O_Moderator at: 11/28/2013 1:48 PMcontact data deleted |
|
11/28/2013 1:52 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread talking with dlms-cosem protocol Best regards O_Moderator |
Follow us on