5/4/2012 11:43 AM | |
Joined: 9/23/2005 Last visit: 3/24/2023 Posts: 4180 Rating:
|
Hi Gabriel, at this momment the CPU 1215C is a intranet topic yet , and there is not so mutch information avaliable (http://support.automation.siemens.com/BR/view/en/59885751) What I can forward to you is that the CPU comes with FW 3.0, will accept FW upgrade without SD card (by Ethernet) but I don't found any changes of Axis behavior (So, I supouse that there will no axis interpolation). Better is to wait up to official delivery release, and see a complet and official information about it. |
Denilson Pegaia |
|
This contribution was helpful to
1 thankful Users |
5/7/2012 10:07 PM | |
Joined: 2/16/2011 Last visit: 3/23/2023 Posts: 229 Rating:
|
Thanks a lot Reagards
|
Gabriel de Oliveira |
|
Follow us on