Industry Online Support
Technical Forum
1/31/2010 5:52 PM | |
Joined: 4/6/2006 Last visit: 1/21/2019 Posts: 604 Rating:
|
Hi Iwan, Sorry for my late response. With the License you have you can communicate directly with the IM151-3PN devices but not with a controller like a S7-400. This would mean you need to create an OPC Client yourself to control the processes now done with the S7-400. There is some more information available via this link: Information about SOFTNET PN IO But for your system setup SIMATIC NET Softnet for Industrial Ethernet (Lean if less then 8 connections) is the better solution. With this license you are able to setup a S7-Connection to your S7-400 and get all the data from the S7-400. |
Best regards, |
|
2/1/2010 9:03 AM | |
Posts: 19 Rating:
|
Ins Thank you for the information. Iwan |
Follow us on