4/15/2016 7:47 AM | |
Joined: 5/11/2010 Last visit: 3/7/2025 Posts: 90 Rating:
|
hi, here I simply tested by RT transfer, it is working... |
4/15/2016 10:33 AM | |
Joined: 5/28/2008 Last visit: 3/23/2025 Posts: 4518 Rating:
|
Hello, Yes it's possible only in this case. But if not, there is no way except one of the following two alternatives:
There's a way to check if the downloaded file on the Panel contains the configuration file or not and can be found the way in the following link. Another important note, Most of the SIMATIC Panels have limitations on their internal memory. So, if the user enabled the option of back transfer, he should use external memory media as indicated in the attachment of the link bellow: How do you back transfer the projects of an operator panel and what should you watch out for? |
Ayman Elotaify |
|
6/23/2016 11:51 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by Dany Min is split to a separate thread with the subject Downloaded to HMI without enabling backtransfer check box, have I to build new application software from scratch?. Best regards |
Follow us on